Altra Motion is a premier global designer and producer of a wide range of motion control and power transmission solutions. With engineered components and systems that provide the essential control of equipment speed, torque, positioning, and other functions, Altra products can be used in nearly any machine, process or application involving motion. Our products are marketed under a variety of well recognized and established brands.
With more than 125 years of frontline experience, Boston Gear is recognized globally as a premier resource for extremely reliable, high-performance power transmission components. Boston Gear offers the industry's most comprehensive product array featuring more than 30,000 standard products combined with the ability to custom engineer unique solutions when required. Product lines include standard enclosed gear drives, custom speed reducers, AC/DC motors, DC drives and Centric brand overload clutches and torque limiters.
Long-lasting Boston products are hard at work in key markets including food processing, material handling, corrugating machinery and packaging equipment in applications such as conveying, filling, labeling, sealing, cartoning, bagging, wrapping, palletizing, component handling, capping, and tensioning.
_________
Founded in 1927, Warner Electric has grown to become a global leader in electromagnetic clutch & brake solutions. Warner engineers utilize the latest design, materials and manufacturing technologies to develop easy-to-use-and-install clutches and brakes with longer life and improved accuracy and repeatability. Warner Electric offers the broadest selection of industrial clutches, brakes, controls, web tension systems, sensors and switches available from a single manufacturer.
Reliable Warner Electric components are used in a wide range of markets including material handling, packaging machinery, food & beverage, elevator & escalator, turf & garden, agriculture and off-highway, forklift, crane and motion control. Applications include conveyors, lift trucks, wrapping machines, servo motors, capping equipment, combines and balers, baggage handling systems, military vehicles, hoist drives and lawn mowers.
_________
For more than 50 years Formsprag Clutch has been known as the world’s leading authority for the design and manufacture of long-life overrunning clutches, backstops, bi-directional clutches and clutch couplings. Formsprag offers the broadest range of both sprag and ramp & roller type overrunning clutches and backstops available globally. Exceptionally reliable Formsprag solutions are hard at work in many key markets including mining, aerospace & defense, packaging equipment, food processing, material handling and paper converting machinery on applications such as conveyors, rotary & fixed wing aircraft, pumps, hoists & cranes and machine tools.
_________
Founded in 1857, TB Wood’s has grown to become a global leader in the design and manufacture of industrial couplings and belted drive solutions. Highly engineered TB Wood’s coupling products, including Sure-Flex® and Dura-Flex® elastomeric couplings, Form-Flex® disc couplings, G-Flex grid couplings, and Jaw couplings, represent the latest in coupling technology, featuring superior design and exceptional quality to ensure long-lasting performance.
TB Wood’s also offers a wide range of innovative, high-performance belted drive solutions including V-belt sheaves, synchronous sprockets, made-to-order sheaves, belted mechanical variable speed drives, belts, and bushings. All TB Wood’s sheaves are constructed of fine grain, high tensile cast iron and have been carefully engineered for long life.
Reliable TB Wood’s products are utilized in many key markets including food & beverage, energy, wastewater, concrete, metals, pulp & paper, and material handling, on applications such as conveyor systems, rolling mills, pumps, compressors, palletizers, de-barkers, printing equipment, fans & blowers, machine tools, and mixers.
_________
For more than 40 years Inertia Dynamics has been recognized as a global leader in the design and manufacture of technically-advanced industrial clutches and brakes. Inertia’s experienced design and development team utilizes sophisticated test equipment to ensure very high quality and consistency levels to meet the most demanding customer requirements. Inertia Dynamics offers a full line of electromagnetic clutches and brakes, wrap spring clutch/brakes, motor brakes, controls and moment of inertia measurement equipment. Long-life Inertia Dynamics products are hard at work in various markets including material handling, food processing, turf & garden and packaging machinery on applications such as conveyors, lawn tractors, filling and cartoning machines and mixers.
________
Ameridrives began manufacturing in 1928. Through the years, Ameridrives has become a pioneer and global leader in advanced coupling technologies that compensate or minimize the effects of unavoidable misalignment and end movement of coupled shafts. Utilizing advanced testing, analysis and manufacturing processes, Ameridrives provides highly engineered coupling solutions to meet challenging customer requirements.
Ameridrives offers a wide range of products including Amerigear gear couplings and mill spindles, high-performance Ameriflex® diaphragm and Ameridisc® couplings, TurboFlex GC® disc couplings, and a full line of Americardan universal joints. Extremely reliable Ameridrives products are hard at work in key industries including power generation, oil & gas, metals, textiles, energy, off-highway, and mining on applications such as gas and steam turbines, compressors, generators, fans & blowers, pumps, crushers, marine/offshore platforms, rolling mills, cranes, irrigation systems, shredders, draglines and shovels.
_________
Founded in 1922, Kilian has grown to become one of the world’s largest producers of precision-machined bearings and value-added assemblies. Extensive application expertise and value-engineering capability allows Kilian to provide unique, cost-effective bearing solutions that meet specific customer needs around the globe. Kilian offers a broad range of bearing solutions including ball, roller, needle and thrust bearings, stainless steel and plastic bearings, track roller bearings, no-rust housed bearings, pins & shafts and polymer assemblies.
Kilian products are used extensively in the automotive market on applications such as steering columns, seating systems, transmission/transfer cases and sliding door hinges. Other industrial applications include appliance hinges, aircraft cargo rollers, tractor seats, recliners, drawer slides and overhead & blue steel conveyors.
_________
Wichita Clutch, founded in 1949, is a leading global designer and manufacturer of heavy-duty clutches and brakes that are essential components in industrial process equipment. Backed by extensive application experience, Wichita engineers utilize the latest design technologies and materials to provide innovative clutch and brake solutions that precisely meet their customer’s most demanding requirements. A full range of Wichita solutions, including hydraulic clutches and brakes, air clutches, air brakes, water-cooled clutches and brakes, and fluid couplings, are used extensively around the world by major OEMs in metalworking, steel, marine, pulp & paper, material handling, mining, and energy.
_________
For more than 70 years, Guardian has been designing and manufacturing world-class couplings and other power transmission components. Utilizing advanced manufacturing technologies and processes, Guardian provides highly-reliable coupling and component solutions to meet the most challenging industrial application requirements.
a