Sign In Or Register
Back to Menu
Back to Menu
Back to Menu
QUOTES
OVERSTOCK SAVINGS
QUICK ORDER
Nachi BMBU Series Angular Contact Ball Bearing
Nachi Logo230x.png

Nachi BMBU Series Angular Contact Ball Bearings

Overheating & Early Failure - Some customers report overheating & early failures due to poor oil flow with larger sized angular contact ball bearings utilizing Inner Ring Guided Cages. These problems are most commonly seen in vertical shaft pumps/gearboxes where the moving components are
designed to be lubricated by a method called “splash lubrication". This relies on rotating components (bearings/gears) to splash & fling oil up towards other moving parts that aren't close enough to the main oil reservoir.

Nachi’s New BMBU Series - Nachi now offers our new BMBU series of 40° Angular Contact Ball Bearings which was designed specifically to improve lubricant flow & cooling efficiency throughout the bearing or bearing set. The new BMBU conical shaped Ball-Guided Cage acts as a turbine when submerged in oil, which pumps the lubricant through a set of stacked bearings or out towards other components. This greatly improves overall lubrication and reduces heat via liquid cooling. The newly designed BMBU Inner & Outer Rings are counter-bored to increase the amount of oil that can flow through the front & back faces of the bearings.

Contact your nearest BDI location for more information about Nachi's new BMBU Series Angular Contact Ball Bearings or view PDF.
 

Nachi-BMBU-Series_w.jpg