SKF Solid Oil Bearings
How do we break the cycle of "We have always done it this way?" How much are you losing from improper bearing lubrication? What is the total cost in labor, grease and downtime? As much as 40 percent of premature bearing failures in the food industry are due to improper lubrication. These environments also introduce potentially damaging food particles that can quickly destroy conventional bearings. Plus, conventional re-greasing and automatic lubrication systems can introduce the potential for food contamination.
Is there a better, more cost-effective solution to meet your needs? The answer is yes! SKF® Solid Oil encapsulated lubrication, which can be applied to virtually any bearing. Solid Oil uses a polymer matrix saturated with lubrication oil that completely fills the internal space and encapsulates the cage and rolling elements. Solid Oil keeps more lubricant on the bearing surface than a corresponding greased bearing...in some instances up to 4 times as much!
Break the cycle of "We have always done it this way" and talk to your BDI representative today about SKF Solid Oil encapsulated lubrication or view PDF.