Renold Jeffrey Engineering Class Drive Chains run some of the most demanding applications in the world. These hard-working chains are found in construction, mining, and power transmission equipment. Renold has over 130 years of experience designing and crafting high-quality engineering drive chains that are built with pride in the U.S.A.
Renold Jeffrey drive chains feature bushings that are machined from solid steel or formed from cold drawn steel and then securely locked by press fits. This ensures that wear is limited to the hard surfaces, extending the life of the chain. Renold Jeffrey drive chains have solid-steel heat-treated pins increase the wear life of the chain. You can count on Renold Jeffrey drive chain to deliver plenty of reserve strength to handle day-to-day operations as well as to stand-up to high shock loads.